Technical FAQs

Ask a Question

Are there Windows or Linux drivers for the NBAC0226 USB to serial cable.

Issue:

There are no drivers available for the NBAC0226 serial to USB cable.

Product Line:

NetBotz

Environment:

NetBotz Serial devices

Cause:

The NBAC0226 Is meant to connect certain serial devices to NetBotz appliances by means of their USB connection

Resolution:
This USB to serial converter is only meant to connect serial devices to a NetBotz appliance. It is not meant as a Windows or Linux Serial to USB converter. There are no drivers available for this cable. 
Was this helpful?
What can we do to improve the information ?