Technical FAQs

Ask a Question

How to access the Installer menu on a EcoBreeze Expansion Module.

                                                                                                                                                           

Issue:   
How to access the Installer menu on a EcoBreeze Expansion Module

Product line:
ACEC200, ACEC201 

Environment:  
All serial numbers 

Cause:  
Install 

Resolution:  

 

To access the Installer menu: 

• Select the PA variable, 

• Press the ENTER button and enter the password value using the UP/DOWN button 

• Confirm the value by pressing the ENTER button. 

• Finally, press and hold down the UP and DOWN buttons for 4 seconds. At this point, the user can scroll through all of the selectable parameters by pressing

the UP/DOWN button. To quit the procedure: 

• Press and hold down the UP and DOWN buttons for 4 seconds, do nothing for 60 seconds, or press the ESC button.

Was this helpful?
What can we do to improve the information ?