Technical FAQs

Ask a Question

What is the range of entering fluid temperatures allowed for the InRow ACRD2XX fluid-cooled unit?

Issue:
What is the range of entering fluid temperatures allowed for the InRow ACRD2XX fluid-cooled unit?

Product line:
ACRD2XX

Environment:
All Versions.

Cause: Install

Resolution:
Each InRow RD fluid-cooled unit functions in a range of 55F – 110F. Additional guidance on temperature ranges can be obtained from the Applications Engineering team.

 
Was this helpful?
What can we do to improve the information ?