Technical FAQs

Ask a Question

NetBotz v3 | How do I enable/disable SNMP?

Issue:
Issues connecting serially to a v3 NetBotz appliance.

Product Line:
NetBotz v3 Wall Appliance: 355/356 (NBWL0355/6) & 455/456 (NBWL0455/6)
NetBotz v3 Rack Appliance: 450/451 (NBRK0450/1), 550 (NBRK0550), & 570 (NBRK0570)

Environment:
NetBotz v3 (all versions)
NetBotz v2 (all verisons)

Resolution:

Enable SNMP on a v3 NetBotz Appliance

1) Download and install the Advanced View Application.  Instructions for download can be found in knowledge base FA230223.
NOTE: If Advanced View is already installed, skip step 1.

2) Log into your NetBotz appliance as an administrator using the Advanced View application.

3) Select the Configuration tab and then under Appliance Settings navigate into SNMP.

4) Check the box for Enable SNMP agent.

5) Fill out the information within Version 1/Version 2c or Version 3 tabs.
NOTE: SNMPv3 settings are based on user profiles.  For user profile configuration see knowledge base FA323442.

6) Select OK to save the settings.


Disabling SNMP 

1) Download and install the Advanced View Application.  Instructions for download can be found in knowledge base FA230223.
NOTE: If Advanced View is already installed, skip step 1.

2) Log into your NetBotz appliance as an administrator using the Advanced View application.

3) Select the Configuration tab and then under Appliance Settings navigate into SNMP.

4) Uncheck the box for Enable SNMP agent.
NOTE: Specific SNMP portocol versions can not be individually enabled/disabled.  SNMP is either enabled/disabled as a whole protocol.

6) Select OK to save the settings.
Was this helpful?
What can we do to improve the information ?