Technical FAQs

Ask a Question

NetShelter CX Air Filters are Difficult to Install.

Issue:
NetShelter CX Air Filters are Difficult to Install.

Product Line:
NetShelter CX

Environment:
AR4038IA serial range: 6N1514J00003
AR4038A serial range: none reported yet but possible.

Cause:
An incorrectly sized joining plate obstructs the air filters on the top of the cabinet. The bottom air filter is fine.

Resolution:
Please contact APC Tech Support.
If you have one of the affected units we can supply a replacement joining plate that's user replaceable. Instructions are attached below so you can see them before hand.
Please have the serial number available when you call. We will assess the case. If it appears to be one of the affected units we will send the customer a replacement joining plate with instructions to swap it out.

APC Tech Support: please see the Internal Kbase document FA245501 for instructions on providing a replacement joining plate: http://www.apc.com/us/en/faqs/FA245501/
Was this helpful?
What can we do to improve the information ?