Technical FAQs

Ask a Question

How many networking cables can a NetShelter CX accommodate?

Issue:
How many networking cables can be run into the NetShelter CX cabinet?

Product Line:
NetShelter CX
 
Environment:
All versions and serial ranges.
 
Cause:
Customers need to know the correct number of cables that can enter/exit the cabinet. 
 
Resolution:
Each cable port can accommodate ~400 Cat 6 cables. (The 38U cabinet has two cable ports, one at the top rear and one at the bottom rear).
 
Was this helpful?
What can we do to improve the information ?