Technical FAQs

Ask a Question

Power Specifications for NetBotz Version 1 Appliances

Issue:

Power Specifications for NetBotz Version 1 Appliances

Product Line:

NetBotz

Environment:

NetBotz Version 1 Appliances

Cause:

Power specs

Resolution:

Power Specifications for Version 1 Appliances :

-The electrical specifications listed below for the all of the units 303, 310 and 400 (Wall and Rack units).

-Input Voltage- (Universal Power Supply) : 90 To 264 VAC

-Supply receptacle - IEC60320, C13

-Input Voltage (US power supply) : 100 - 240 VAC

-Input power in VA : 4W Typical

-Current ( @ 100V): 40mA Typical

-Heat dissipation in BTU: 14 BTU / Hour
 
Was this helpful?
What can we do to improve the information ?