USA/EN - Choose Country or Region
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
When to replace your battery or UPS
UPS Buying Guide
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
USA/EN - Choose Country or Region
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
GPS Receiver Support for the NetBotz 500
Issue:
GPS Receiver Support for the NetBotz 500
Product Line:
NetBotz
Environment:
Version 2 NetBotz 500
Cause:
Supported configurations..
Resolution:
The NetBotz 500 supports the attachment of a GPS (global positioning system) receiver.
The NetBotz 500 reports GPS readings such as latitude, longitude, altitude, heading, velocity, and status as monitorable sensors
Current latitude and longitude readings can be attached to all alerts
Connects to WB500 USB port using USB-to-RS232 serial converter cable
Support for two NMEA-compliant GPS receivers:
Garmin GPS35 USB
Laipac G10-USB