Technical FAQs

Ask a Question

Unable to Login to NetBotz Central 1.x via SSL

Issue:

Unable to Login to NetBotz Central 1.x via SSL

Product Line:

Netbotz Central

Environment:

NetBotz Central 1.x

Cause:
SSL Certificate Mismatch

Resolution:

Unable to Login to NetBotz Central 1.x via SSL

If a NetBotz Central 1.x server is configured for incorrect SSL parameters an error may occur when attempting to login. The error message text will be: "Certificate Mismatch" error occurs.

To work around this problem, perform the following steps:
In the "C:\Program Files\netbotz" subdirectory edit the nbc.bat file.
On the last line of that fine, place a "-s" right before the "%y%". This will force the console to work in non-SSL mode
Was this helpful?
What can we do to improve the information ?